To set a timeout period for trigger events that occur during a sequence, click the checkbox and set a value in ms.
This parameter should be set to a value that exceeds the trigger arming period (the time between the previous acquisition completing and the next trigger).
If the triggers for all acquisitions in the sequence are set to Free Run, the Trigger Timeout is ignored.